Search FAQs
Can the cables used with XY2CH and XY2CE emergency stop trip wire switches be turned through angles or must they be straight?
The cables used to operate XY2CHxxx and XY2CExxx emergency stop cable pull switches may be installed turning through angles by using the specified pulleys (XY2CZ708). There are two important rules to follow:
Caution: This FAQ references XY2CH and XY2CE only. Other rules apply for other XY2C ranges.
- Maximum number of angles / deviations: 2
- Combined sum of the two internal angles must be equal to or greater than 180°. See below diagram taken from the instruction sheet:
Caution: This FAQ references XY2CH and XY2CE only. Other rules apply for other XY2C ranges.
Released for:Schneider Electric Ireland
Explore more
Range:
Explore more
Range: