Search FAQs
Can I connect a Magelis display unit directly to a Zelio programmable relay module?
It is now possible to link HMISTO705 (and now obsolete HMISTO501) to the Zelio Logic smart relays via the communication protocol.
The communication cable for Zelio Logic, SR2CBL09 is dedicated for this communication. This cable is used to connect the programmable module's integrated port to the HMI. No external Modbus communication module is therefore required to implement this solution.
The diagram below shows the options:
![Connection image](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000D3syTQAR&oid=00DA0000000abSmMAI)
The Software for the now obsolete HMISTO501 was Vijeo Designer.
The communication cable for Zelio Logic, SR2CBL09 is dedicated for this communication. This cable is used to connect the programmable module's integrated port to the HMI. No external Modbus communication module is therefore required to implement this solution.
The diagram below shows the options:
Further information about the software of the HMISTO705 can be found in this FAQ:
https://www.se.com/uk/en/faqs/FAQ000229667/
The Software for the now obsolete HMISTO501 was Vijeo Designer.
Released for:Schneider Electric Ireland
Explore more
Range:
Explore more
Range: