{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Do the Acti9 Single phase Split metered boards (SEA9APN14S14 , SEA9APN10S10 & SEA9APN6S6) come with incomer and meters fitted?
Yes the the Acti 9 Single phase split metered boards (SEA9APN14S14, SEA9APN10S10 & SEA9APN6S6) come with incomer and two meters fitted as standard.

SEA9APN14S14 comes with 125A DP switch, 2 x 50A DP MCB and 2 x meters A9MEM2105
SEA9APN10S10 comes with 125A DP switch, 2 x 50A DP MCB and 2 x meters A9MEM2105
SEA9APN6S6 comes 125A DP switch, 2 x 40A DP MCB and 2 x meters A9MEM2010

Schneider Electric Ireland

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: