{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to define the part number of NSX current transformer?
First you need to define the type of current transformer, of which we offer three types.

- Solid CT
- Bolt on CT
- Split Core CT

For more information on solid CT , then check the attached Acti9 catalogue in which you can find in section 7 Control and command page 98 to page 108.

Example Current Transformer (CT)


For more information on bolt on CT which is the direct connected Ct,s that fit to the NSX MCCB, the attached document Section 8 Powerpact 4 Panelboards, page 17 of the Acti9 catalogue.

Two options are available as listed below, one is with voltage references and the other is without

The factors to take into account here are the amount of available space in the MCCB panel, current to be measured and how many poles are required to be monitored. If this method is used then there are two types of facility that the Ct can offer see diagram below.


Selection of CT's

For the Split Core CTs see attached the Veris split core CT sheet showing various sizes referring to current ratio.

Schneider Electric Ireland

Attachment(s)
SE8863__8_Powerpact_4_Panelboards.pdf [1.12 MB]
SE8863__7_Control_&_Command-PART2.pdf [3.94 MB]
Veris split core CT.pdf [507.36 KB]
Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: