Can you tell me what the hole centers are for the screws to mount on Ultimate Grid Plates.
The hole centres for screws are the standard 60.3mm (1 gang) and 120.6mm (2 gang). Grid front plates are screwed to the frames (or clipped if Ultimate Screwless).
See datasheet for Grid Plates attached.
Released for:Schneider Electric Ireland
Attachment(s)
Data sheet - Ultimate grid overview.pdf [74.62 KB]
Explore more
Range:
Software - DS ConneX
Ultimate
Articles that might be helpful
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.