{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the amount of SF6 gas in Ringmaster RMU?

Data on SF6 gas amount in Ringmaster Ring Main units and Ringmaster Range units.
For older units please contact Schneider Electric.

Ringmaster RMU
RN2d / RN6d   weight 592 g.
RE2d / RE6d   weight 703 g.
Pressure bar G 0.55

Ringmaster Range RMR switch
SN6 / SE6   weight 493 g.  pressure bar G 0.35

Ringmaster Range RMR circuit breaker
CN2 / CE2 / CE6   weight 493 g.  pressure bar G 0.55

Amount of SF6 gas inside unit always is indicated on the unit rating plate.

Schneider Electric Ireland

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: