{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Insulation Resistance Test on USB sockets

This would not be advisable to perform a 500V resistance test on the USB sockets.
"Insulation resistance test cannot be performed on the USB sockets as the electronic circuitry inside the SMPS could easily be damaged by a 500 V insulation test injected across it. Consequently the USB port may fail to function following a 500 V Line to Neutral insulation test. Hence it is not recommended but the all the insulation resistance for the socket USB is as per EN 60950-1 & BS 5733."
Ultimate Screwless Flateplate USB twin socket

Schneider Electric Ireland

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: