Search FAQs
What is the operating ambient temperature range for Ringmaster?
Standard Ringmaster units can be installed in environments which meet ‘normal service conditions’ as defined by IEC 62271-200, 62271-1 section 2.1.
Ambient temperature: -25°C to +55°C
Altitude: up to 1,000 meters above sea level.
More information is available on Ringmaster web page .
Ambient temperature: -25°C to +55°C
Altitude: up to 1,000 meters above sea level.
More information is available on Ringmaster web page .
Released for:Schneider Electric Ireland
Explore more
Range:
Explore more
Range: