{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Do we offer a 3 pole RCBO in Acti 9
Schneider do not offer a 3 pole RCBO in the UK
However, it is possible to achieve a 3 pole RCBO but it has to be built from a 3 pole MCB and a Vigi unit fitted on the side.
For example a 3 pole, 16A , 30mA RCBO will comprise of parts A9F54316 + A9V02763 but the device will now be 6 module wide not 3.

We only offer the Vigi units in 30mA and 300mA but they will fit on any Acti 9 MCB, 3 pole device up to 63A.

Schneider Electric Ireland