{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why does my circuit breaker keep tripping when the blinds change direction?
When you shut off of a single phase motor followed by a quick change in direction, it can cause the motor to work harder because of the change of direction.
This causes the motor to consume a larger amount of current (it has a larger inrush current).
The reason why it consumes a larger amount of current is because the motor is in the process of reversing its magnetic poles which is accomplished by reversing the polarity of the starter winding.
This may be enough current to trip some Circuit breakers.
Failure to extend the change over time may result in the motor burning out, or consistent nuisance tripping of a circuit breaker.
Or potentially even the motor not reversing direction.
By increasing the “change over delay” to meet the blind manufacturers specifications should prevent any of these issues from happening.

Schneider Electric Ireland

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: