To use trigger functions this would need to be setup on another device EDLT/Saturn/Paca etc.
Create the scene on the other device setting on and off or percentage, then select the Trigger group and create two action selectors. 0 to 255
Once done this move to Saturn device and make sure this has no scenes on the device, set the secondary application to trigger then select trigger group with an on /off function upload this to network and this will activate the button to be used as two scenes as long as no duplicate trigger or scene on devices.
Create the scene on the other device setting on and off or percentage, then select the Trigger group and create two action selectors. 0 to 255
Once done this move to Saturn device and make sure this has no scenes on the device, set the secondary application to trigger then select trigger group with an on /off function upload this to network and this will activate the button to be used as two scenes as long as no duplicate trigger or scene on devices.
Released for:Schneider Electric Ireland