Search FAQs
What is the life span of the XVB LED tower light?
The lifespan for the lamp used in the XVB range of tower lights, DL1BDB1, is as follows:
Normally, it will be over 100,000 hours. However, the brightness will be decreased over the course of the LED's working life.
We define the light output efficiency for end of life is less than 70%, therefore the lifetime of LED light is approximately 70,000 hours. This equates to nearly 8 years if illuminated continuously.
Normally, it will be over 100,000 hours. However, the brightness will be decreased over the course of the LED's working life.
We define the light output efficiency for end of life is less than 70%, therefore the lifetime of LED light is approximately 70,000 hours. This equates to nearly 8 years if illuminated continuously.
Released for:Schneider Electric Ireland
Explore more
Range:
Explore more
Range: