Search FAQs
How do you check if the NW Breaker has been manufactured with a Restricted Earth Fault (REF)
To check if an NW breaker is manufactured with the REF: Restricted Earth Fault look at the Bill of Materials (BOM)
The Bill of Material (BOM) must include the reference 64877. Description (Restricted Earth Fault Option).
The Bill of Material (BOM) must include the reference 64877. Description (Restricted Earth Fault Option).
Released for:Schneider Electric Ireland
Explore more
Range:
Explore more
Range: