Search FAQs
How much space do I need around a GenieEvo switchgear?
GenieEvo should be installed in a clean, dry, well ventilated substation whose climatic conditions are controlled to stay within those specified in IEC 62271-200 clause 2.1.1. GenieEvo has been tested to IEC 62271-200 for internal arc classification AF and requires the following minimum dimensions:
For more information please see Installation, operation and maintenance instructions .
- From back of switchboard to rear wall - 800mm
- From end of switchboard to side wall - 500mm
- From floor to ceiling - 3000mm
For more information please see Installation, operation and maintenance instructions .
Released for:Schneider Electric Ireland
Explore more
Range:
Explore more
Range: