{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the internal arc withstand for an RM6 cubicle?

RM6 switchgear has been designed to withstand the impact of an internal arc. Stainless steel tanks and cable boxes are fully internal arc rated according to standard IEC 62271-200. If a RM6 cubicle is equipped with a special LRU (internaL arc Reduction Unit) “filter”, internal arc classification IAC is AFLR 20kA 1s.
Please contact Schneider Electric for different internal arc options.

Schneider Electric Ireland

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: