Search FAQs
Should I use the adapter for phase comparator on an 24kV SM6 cubicle?
The 3723912 comparator can be used (PDU and VPIS) up to 7.2 kV.
Between 10 and 24 kV there are two options: PDU/VPIS: use the 3730139HC adaptor in addition. VPIS/VPIS: the comparator can be used on its own. The 3723912 comparator is suitable for all cases apart from PDU/VPIS between 10 and 24 kV.
Between 10 and 24 kV there are two options: PDU/VPIS: use the 3730139HC adaptor in addition. VPIS/VPIS: the comparator can be used on its own. The 3723912 comparator is suitable for all cases apart from PDU/VPIS between 10 and 24 kV.
Released for:Schneider Electric Ireland
Explore more
Range:
Explore more
Range: