Search FAQs
What material is used for the enclosures of the VCF*GE or VCFXG** type Vario switch disconnectors?
The enclosure bases and covers of enclosed VARIO switch-disconnectors, part numbers VCF*GE or VCFXG**, are made of Makrolon 6385. The fire resistance of this material is as follows:
- 960 Deg C according to standard IEC 695-2-1
- V0 according to standard UL94
- I3F1 according to NF F16-101
Released for:Schneider Electric Ireland
Explore more
Range:
Explore more
Range: