undefined [object Object]
{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Which Square D pressure switches are still available?
Many issues relating to ordering Square D pressure switches, are to do with the part numbers. Most of the original Square D part numbers are still used, e.g. 9013FSG2J24.

In some cases, the references have been altered slightly for ordering purposes - e.g. 9012ACW1M11 is now ACW1M119012. Note that this is just a reformatting of the part number (class number - 9012 in this case - is moved from the start to the end), and has no effect on the product it-self.

Should the switch you require appear to be unavailable then, in the UK, contact Technical Support by chat or by other means (www.se.com/uk or through My Schneider), and we will help you determine if the original product can be obtained or suggest a possible alternative.

Note that, unless you have a direct purchasing account with Schneider Electric, you will need to buy through a distributor / wholesaler. You can find more information in the Support tab on our website.

Schneider Electric Ireland

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: