The GV2AF3 fits between the TeSys D contactor and the TeSys GV2 Motor Circuit Breaker (MCB). The Tesys D contactors have different coil dimensions making the DC coils taller than the AC coil versions, which can cause problems when mounting using GV2AF3.
This short video shows how to set up the GV2AF3 for DC and AC coils. It also shows how to mount the TeSys D to the GV2AF3 and to a TeSys GV2.
GV2AF3 can be used with any of the GV2 range (GV2ME, GV2P etc.)
This short video shows how to set up the GV2AF3 for DC and AC coils. It also shows how to mount the TeSys D to the GV2AF3 and to a TeSys GV2.
GV2AF3 can be used with any of the GV2 range (GV2ME, GV2P etc.)
Released for: Schneider Electric Ireland