Search FAQs
How to program the Harmony XB5/XB4 Wireless Pushbutton as a Start-Stop function
The Harmony XB4 and XB5 programmable Wireless push buttons are very adaptable
If you have two pushbuttons and the receiver XBRRA, they can be programmed to operate as a start / stop set.
The video below shows the process of setting this function:
Also attached is a programming guide that covers most of the functions of the XB4R and XB5R range
The following items were used in the video:
If you have two pushbuttons and the receiver XBRRA, they can be programmed to operate as a start / stop set.
The video below shows the process of setting this function:
Also attached is a programming guide that covers most of the functions of the XB4R and XB5R range
The following items were used in the video:
- ZBRRA Configurable Receiver (with Output Functions: Monostable, Bistable, Start / Stop)
- ZB5RTA4 Red Flush Push button (Plastic)
- ZB5RTA5 Black Flush Push button (Plastic) (Note: it would be more normal to use a Green push button ZB5RTA3 for the start function)
- ZBRM22 Plastic Enclosure (2 cut outs)
Released for:Schneider Electric Ireland
Attachment(s)
Explore more
Range:
Explore more
Range: