{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How do you setup an ATV Process drive with an M221 with Modbus TCP control
Below is a video showing the steps in SoMachine Basic (now it is called EcoStruxure Machine Expert Basic) on how to set up an interface between an ATV Process Drive and an M221 Controller

This process presumes that you have set up a TCP/IP network and give the IP Adress to the ATV Drive.



Inside EcoStruxure Machine Expert Basic (former SoMachine Basic) we have the possibility to use function blocks to control the Altivar drive.
Please find attached an example project and the Library guide.

Schneider Electric Ireland

Attachment(s)
EcoStruxure Machine Expert Basic - Function Blocks ATV.pdf [331.76 KB]
_M10.4 IO Scanner Modbus TCP for ATVs (ETH_DIRECT).smbp [246.49 KB]
How do you setup an ATV Process drive with an M221 with Modbus TCP control
Below is a video showing the steps in SoMachine Basic (now it is called EcoStruxure Machine Expert Basic) on how to set up an interface between an ATV Process Drive and an M221 Controller

This process presumes that you have set up a TCP/IP network and give the IP Adress to the ATV Drive.



Inside EcoStruxure Machine Expert Basic (former SoMachine Basic) we have the possibility to use function blocks to control the Altivar drive.
Please find attached an example project and the Library guide.

Schneider Electric Ireland

Attachment(s)
EcoStruxure Machine Expert Basic - Function Blocks ATV.pdf [331.76 KB]
_M10.4 IO Scanner Modbus TCP for ATVs (ETH_DIRECT).smbp [246.49 KB]
Explore more
Range:
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Explore more
Range:
move-arrow-top