The models detailed below can have sounds programmed and stored on the tower light using a SD memory card:
To download the latest version:
There are a total of 3 products that use the Playlist Builder software tool. They are the two mentioned above, XVUC9V, XVUC9VP, and the XVSV range.
Below is a video that gives an example of programming and installing sounds on to the beacon
- XVUC9V
- XVUC9VP
To download the latest version:
- Go to www.se.com/uk
- Click on the "Support" tab
- Click on "Products, Documents & Software"
- Search for "playlistbuilder" to get the latest version
There are a total of 3 products that use the Playlist Builder software tool. They are the two mentioned above, XVUC9V, XVUC9VP, and the XVSV range.
Below is a video that gives an example of programming and installing sounds on to the beacon
Released for:Schneider Electric Ireland