{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can 80A or 100A miniature circuit breakers be fitted onto the outgoing ways of the Acti9 Isobar Distribution Boards?

The Acti9 Isobar Distribution Boards outgoing ways are designed to be fitted with iC60H MCB's up to and including 63A.

MCB's rated at 80A and above are physically larger and do not fit the isobar busbar system.

However , there is a way around this -

By installing a SEA9BNEX034N below the board and fitting an 80A iC120H MCB in this enclosure you can then feed from the board (via an SEA9TB1001) terminal block in to the iC120H

For single pole MCB's use 1 x SEA9TB1001 for 3 pole MCB's use 3 x SEA9TB1001.

Schneider Electric Ireland

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: