{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can a Contactor be fitted on to the outgoing way of an Isobar 4c/Acti9 Isobar Distribution Board?

The Isobar 4c and Acti9 Isobar Distribution Boards outgoing ways are designed to be fitted only with C60H and iC60H MCB's up to 63A and RCBO's up to 45A

Contactor's and other DIN rail devices cannot be fitted.

They should be fitted on a DIN rail in an enclosure above or below the board

In the case of single phase boards, a multiservice single phase distribution board has a DIN rail already fitted next to the outgoing ways for you to use for contactors/time clocks or similar

See link below for part numbers on the Multi Service Single Phase Boards

https://www.se.com/uk/en/download/document/SE8863_1/

As for a three phase board an extension box with a DIN rail of 17 single pole ways part number is SEA9BNEX034N for both series of Distribution Boards

Schneider Electric Ireland

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: