Search FAQs
Can a time clock be fitted onto the outgoing way of an Isobar Distribution Board?
The Isobar Distribution Boards outgoing ways are designed to be fitted only with C60H and iC60H MCB's and RCBO's up to and including 63A.
Time clocks and other Din rail devices cannot be fitted as an outgoing device in a distribution board.
They should be fitted on a din rail.
- In the case of single phase boards, a multiservice single phase distribution board has a din rail already fitted
- As for a three phase board, an extension box with a din rail of 17 single pole ways part number is SEA9BNEX034N for Acti9 distribution boards.
Time clocks and other Din rail devices cannot be fitted as an outgoing device in a distribution board.
They should be fitted on a din rail.
- In the case of single phase boards, a multiservice single phase distribution board has a din rail already fitted
- As for a three phase board, an extension box with a din rail of 17 single pole ways part number is SEA9BNEX034N for Acti9 distribution boards.
Released for:Schneider Electric Ireland
Explore more
Range:
Explore more
Range: