{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How do you connect the LTMCU Compact Display to the TeSys T LTMR Controller?

The TeSys T Compact Display LTMCU is connected to the LTMR Controllers via the RJ45 modbus connector on the front of the TeSys T controller or, if an expansion module is fitted, via the RJ45 connector of the Expansion module (LTMEV40BD or LTMEV40FM)

The following connecting cables are available:
LengthPart Number
1mLTM9CU10
3mLTM9CU30






Please watch the video below to see an example of these connections being made:

Schneider Electric Ireland