{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the bend radius of uPVC Perimeter Trunking?

Perimeter trunking 40mm ± 2.0mm deep can be bent to a radii of 6.0m minimum, internal or external. Anything smaller, then the trunking has to be segmented (like 20 or 50 pence coin).

Perimeter trunking 50mm ± 2.0mm deep can be bent to a radii of 7.5m minimum, internal or external. Anything smaller, then the trunking has to be segmented.

Perimeter trunking 60mm ± 2.0mm deep can be bent to a radii of 9.0m minimum, internal or external. Anything smaller, then the trunking has to be segmented.

Schneider Electric Ireland