{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Are Loadcentre KQII products compatible with QO LoadCentre distribution boards?

Unfortunatley not. However, outgoing devices (mcbs and rcbos) are still available for original QO LoadCentre distribution boards.
MCBs are available in C type only from 10amp to 63amp 1,2 or 3 pole
example part number for 3pole 32A = QO332VSC10.
RCBO are available in both B & C type  Example part codes
C type 32a 30ma = QO132C10RCBO30F
B type 16a 30ma = QO116B10RCBO30F

Schneider Electric Ireland

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: