{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can the NG125 range of MCB's be fitted into the Isobar range of Distribution Boards?

The Isobar Distribution Boards outgoing ways are designed to be fitted with only C60H and iC60H MCB's up to and including 63A.

MCB's rated at 80A and above are physically larger and do not fit the isobar busbar system.

It is possible to fit externally a NG125N breaker up to a Maximum of 100A using SEA9TB1001 ( 1 per phase) fitted as outgoing way and then cable into a din rail extension box (SEA9BNEX034N) with the NG125N fitted inside.

Schneider Electric Ireland