{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
With Sepam 80 that use 2 sets of current sensors, is it possible to use LPCT sensors and 1A or 5A CT?
Yes, with Sepam series 80 devices that use 2 sets of sensors, it is possible to connect conventional current sensors (In/5A or In/1A) and/or LPCT sensors.


It is only with Sepam series 80 devices that use transformer differential protection (Sepam T87, M88 and G88) that LPCT sensors may not be used.

Schneider Electric Ireland