{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the minimum overload setting on the Micrologic 2 trip units?

The NSX Micrologic 2 trip unit overload setting is adjustable between 0.36 and 1 times the rating (In) of the device.
The (Io) front dial on the Micrologic trip units are adjustable between 0.4 and 1 times the rating (In) of the device.
Fine adjustment (Ir=Io x  0.9 to 1 ) may be programmed into the trip unit using the keypad.

Schneider Electric Ireland

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: