Search FAQs
Are the iCT range of contactors suitable for motor control applications?
Some of the iCT range of contactors are suitable for motor applications.
They have a Utilization category AC-7a and AC-7b conforming to IEC 61095
Note: The following iCT contactors do not have a AC-7b rating and are not suitable for use in motor control applications
Please look for our Tesys range of motor control contactors and other motor control devices or contact our Industrial Control technical department for further advise.
They have a Utilization category AC-7a and AC-7b conforming to IEC 61095
Note: The following iCT contactors do not have a AC-7b rating and are not suitable for use in motor control applications
- A9C22824
- A9C20882
- A9C22722
- A9C20884
Please look for our Tesys range of motor control contactors and other motor control devices or contact our Industrial Control technical department for further advise.
Released for:Schneider Electric Ireland
Explore more
Range:
Explore more
Range: