{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can I have a SF6 pressure indicator with contact on RM6?

RM6 performance meets the definition of a “sealed pressure system” as laid down in the IEC recommendations.
The stainless steel enclosure with IP67 ingress protection is filled with SF6 at 0.23bar relative pressure and sealed for life after filling.

Manometer or Densimeter with pressure contact is used for SF6 gas pressure monitoring.

Schneider Electric Ireland

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: