Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Which is the default user and password for the Modicon M172?

Article available in these languages: Spanish

If it is the first time you connect to the Modicon M172 via USB cable and the EcoStruxure Machine Expert HVAC asks you for credentials you will need to use this:
User:                  administrator
Password:          password

If you want to connect to the WebServer of the M172 and it asks you for credentials the default is:
User:                  administrator
Password:          password

Schneider Electric Ireland

Explore more
Range:
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Product: