{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What contacts to use with the 9001K joysticks?
In the 9001K joysticks, the contact block to use will be different according with the type of movement.

- 3 positions horizontal movement joysticks such as 9001K30 to 9001K33 will require the contact 9001KA3
- 3 positions vertical movement joysticks such as 9001K70 to 9001K73 will require the contact 9001KA2
- 5 positions joystick like such as 9001K34 to 9001K37 will require the contact 9001KA1

More details on Table 1 (page 2) of the instruction:

https://download.schneider-electric.com/files?p_Doc_Ref=65013-001-21&p_enDocType=Instruction%20sheet

Schneider Electric Ireland

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.