{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the different knockouts sizes available in the empty Easy9 Compact Consumer Unit ?
The details of the knock outs are shown below and are also available in the Catalogue,
Knockout Information
Information CommercialDiameter 32 mm
(E)
Diameter 25 mm
(F)
Diameter 20 mm
(G)
50 x 100 mm
(H)
EZ9E10MCCU8422
EZ9E12MCCU8462
EZ9E16MCCU84103


Easy9 CCU Knockout sizes, quantity, and positions

Schneider Electric Ireland