If you are downloading the application to an HMISTU via "File System" with USB stick and receive the warning message:
"Application has halted due to: In Java Class"
"Retentive variable SRAM backup is removed due to size mismatch."
We have two recommendation to solve that problem:
1) Create a basic project on Vijeo Designer and download it to the HMI via "File System" before downloading the application that you want in the HMISTU.
2) Download your application via Ethernet or USB cable to the HMISTU. Make sure to select the option "Preserve Run-Time Data" and "Delete All Run-Time Data" before the downlod:
If you are using Vijeo Designer v6.2 SP8 along with SoMachine you can update your version to Vijeo Designer v6.2 SP8 HF18 to solve this problem next time you download via "File System".
Contact your local technical support for this version.