{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How wired Arc Fault protection in Isobar?
Acti9 Active and Acti9 iARC have to be installed on a DIN Rail.
Therefore an extension enclosure with a DIN rail is required whatever your installation (retrofit or new one).
The extension enclosure can be placed below or a side of main enclosure.
You can refer to the extension enclosures section listed into the Acti9 Isobar P catalogue.
In case you intent to use the all in one Acti9 Active product, you should add a terminal block in the Isobar panel board ( as described thereafter).

Needs:
1/ Extension enclosure with DIN rail (ex SEA9BNEX034N or SEA9BN8SXS)
2/ Terminals blocks (SEA9TB1001) to supply phase from Isobar to Acti9 Active product
3/ Acti9 Active device

Fig1 Acti9 Active and Acti9 iARC how to wire
fig1


If you intend to use the Acti9 iARC, you must wire it as shown below -

Fig2 iARC how to wire
fig2

Schneider Electric Ireland

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: