{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Which is the software to program the Harmony HMISTO7 range?

The software to program the HMISTO7 range (HMISTO705, HMISTO715 , HMISTO735 is EcoStruxure Operator Terminal Expert (former Vijeo XD ).  The software can be download from the next link:

https://www.se.com/ww/en/product-range/62621-ecostruxure-operator-terminal-expert/#software-and-firmware

After the installation of EcoStruxure Operator Terminal Expert, the trial version of the software is available for 42 days and will have to be
activated with the commercial license. In UK we only have the printed licenses.

Once you have the software in order to download the application to the Harmony HMI we can use a miniUSB cable (TCSXCNAMUM3P or BMXXCAUSBH018).

For more information please access to https://digicat.se.com/  or direct to the catalog:
https://download.schneider-electric.com/files?p_Doc_Ref=DIA5ED2140703EN

If the customer is not interested in the WebServer or the OPC features with the basic license it will be enough HMIEELCZLSPMZZ.

Schneider Electric Ireland

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: