Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Which is the software to program the Harmony ST6 and Harmony STM6 range?
The software to program the Harmony ST6 range is EcoStruxure Operator Terminal Expert (former Vijeo XD ).  
The software can be download from the next link:
https://www.se.com/ww/en/product-range/62621-ecostruxure-operator-terminal-expert/#software-and-firmware

The Harmony ST6 include the next references:
•HMIST6200 ( 4.3" W)
•HMIST6400 ( 7" W)
•HMIST6500 ( 10.1" W)
•HMIST6600 ( 12.1" W)
•HMIST6700 ( 15.6" W)

The Harmony STM6  (modular HMI) include the next references:
•HMISTM6200 ( 4.3" W) + HMISTM6BOX
•HMISTM6400 ( 7" W) + HMISTM6BOX

After the installation of EcoStruxure Operator Terminal Expert, the trial version of the software is available for 42 days and will have to be
activated with the commercial license. In UK we only have the printed licenses.

Once you have the software in order to download the application to the Harmony HMI we can use a microUSB cable like the HMIZG936:
https://www.se.com/ww/en/product/HMIZG936/harmony-st6-usb-transfer-cable/

For more information please access to https://digicat.se.com/  or direct to the catalog:
https://download.schneider-electric.com/files?p_Doc_Ref=DIA5ED2181202EN

If the customer is not interested in the WebServer or the OPC features with the basic license it will be enough HMIEELCZLSPMZZ.

Schneider Electric Ireland

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more