Search FAQs
Where can I find a step (.stp) CAD file for XAPM1502 or XAMP1502H29?
Please note: XAPM1502 and XAPM1502H29 have both been replaced. The nearest replacement is XAPD1502. You can find more information, including CAD files, for this new product on our website www.se.com/uk.
You can find the step file for XAPM1502 attached.
Although we don't have a step file for XAPM1502H29, the only difference is in the cable entry, and so in the majority of cases the same step file can be used for both.
XAPM1502:
XAPM1502H29
You can find the step file for XAPM1502 attached.
Although we don't have a step file for XAPM1502H29, the only difference is in the cable entry, and so in the majority of cases the same step file can be used for both.
XAPM1502:
cable entry | 1 hole with blanking plug for cable gland, clamping capacity: 14 mm 1 hole without blanking plug for cable gland, clamping capacity: 14 mm |
---|
XAPM1502H29
cable entry | 1 hole with blanking plug for ISO 429248 cable gland, clamping capacity: 20 mm 1 hole without blanking plug for ISO 429248 cable gland, clamping capacity: 20 mm |
---|
Released for:Schneider Electric Ireland
Attachment(s)
Explore more
Product:
Range:
Explore more
Product:
Range: