{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the XPSMCMER0002 and XPSMCMER0004 be used with the backplane expansion?
The XPSMCMER0002 and XPSMCMER0004 internal design don't allow the use of the backplane expansion connector. This is mentioned on the module user guide:

User Guide print

The unit uses the same physical case as the other modules but to avoid confusion, it's supplied with a black label covering the backplane cutout (as shown in attached image).

Schneider Electric Ireland

Attachment(s)
Label seal.jpg [480.21 KB]
Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: