{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Which is the software to program the Modicon M241?
The software to program the Modicon M241 is EcoStruxure Machine Expert (former SoMachine). 

In order to install this software you need to download "Schneider Electric Software Installer" from the next link:
https://download.schneider-electric.com/files?p_Archive_Name=ESEMACS10_INSTALLER.zip&p_enDocType=Software%20-%20Release&p_Doc_Ref=ESEMACS10_INSTALLER

Then you should be able to install EcoStruxure Machine Expert.
The software EcoStruxure Machine Expert has a Free version after the 42 days trial, please check pages 14 and 16 for more information for the free version limitations:
https://download.schneider-electric.com/files?p_Doc_Ref=DIA3ED2180701EN

The user that wants to use this software needs to have an account in our License Portal in order to register the software:
https://www.se.com/ww/sites/corporate/en/support/software-licensing/user-login 

In the past the software was SoMachine and the latest version of this software was the SoMachine V4.3 SP2.
The reference for SoMachine is the SOMNACS43:
https://www.se.com/ww/en/product/SOMNACS43/somachine-software-v4-3-usb-drive-format/

The firmware version of the Modicon M241 for PLC programmed in SoMachine starts in v4.0.x.x., the latest version of the firmware for SoMachine v4.3 is the v4.0.6.41 due to hardware changes.
 
The firmware version of the Modicon M241 for PLC programmed in EcoStruxure Machine Expert v1.2.x starts in v5.0.x.x.
The firmware version of the Modicon M241 for PLC programmed in EcoStruxure Machine Expert v2.x.x starts in v5.1.x.x.

If you install the EcoStruxure Machine Expert , please select also the installation of the "Controller Assistant" so you can check this information.

In order to program the Modicon M241 you can use a miniUSB cable (TCSXCNAMUM3P or BMXXCAUSBH018) , a SD Card or an ethernet cable.
 

Schneider Electric Ireland

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.