{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do you fit Acti9 Arc Fault Device (Acti9 Active/iARC) on Isobar P?
Recommended Solution 1:
Acti9 Active AFDDs (iCV40H) can be fitted on Isobar P – Hybrid or Standalone Active distribution boards.
This is the list of AFDDs references that can be used are mentioned below :
  • A9TDFD606
  • A9TDFD610
  • A9TDFD616
  • A9TDFD620
  • A9TDFD625
  • A9TDFD632
They are accessible through the range Acti9 Active : https://www.se.com/uk/en/product-range/45435131-acti9-active/47506957254-products/
Once you have selected the right product, here are the instructions to mount it on Isobar P  - Hybrid  or Standalone Active distribution boards.
Refer to the instruction sheet: See Attached file.

Recommended Solution 2:
Acti9 iARC AFDDs cannot be fitted directly on the pan assembly of Isobar P distribution boards.
It’s recommended to fit on Acti9 Extension Enclosure. For more details refer below:
https://www.se.com/uk/en/faqs/FAQ000222877/

Schneider Electric Ireland

Attachment(s)
GDE66871-00 (1).pdf [5.63 MB]