{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How many modules of devices & how can it be fitted on the AFDD Busbar?
Install Easy9 AFDD on a DIN Rail in an enclosure which is required for installation (retrofit or new one).
You should consider 2 no.s of terminal block(EZ9TB1001)/ 2 pole Switch as an incomer (Phase & Neutral) to the AFDDs for 1 phase supply. The neutral and phase from main switch or Terminal blocks(EZ9TB1001) can be connected directly using the AFDD Comb busbar(SEPNB112) & it is top fed and it is easy to mount.
Image showing installation of AFDD utilizing a terminal block and Isolator
Requirements:
  • Enclosure with DIN rail
  • Terminals blocks (EZ9TB1001) or 2P Switch
  • Easy9 AFDD devices
Easy9 dedicated busbar that can be used in different configurations


Schneider Electric Ireland