{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to connect main row to second row in multirow compact consumer units?
Using the Cable kit (EZ9CCUCABLEKITMR - Inter row Cable kit  for Multirow) the line/phase & neutral from incomer in the main row can be connected to the devices in the other rows along with appropriate device E.g. Terminal block.
Cable kit is flexible to support position of Incomer Switch on Left or Right. For three-row consumer unit, it is recommended to use Terminal Block to connect the cable from second row to third row.

For more details please see the attached information sheet

Additional CRs – Easy9 Terminals block 100A (EZ9TB1001)
Quantity of Cable kits required
Si No.Enclosure TypeCable Kit
Qty to be used
12R CCU - EZ9E212MCCU1
23R CCU - EZ9E312MCCU2

Schneider Electric Ireland

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: