What is the role of the IO module LV434063 and if it is needed for the plug in base NSX MCCBs?
If the plug in base or drawout chassis is equipped with the two position indicating switches (connected/disconnected) then the IO module is needed to present this status information into the communication system. Otherwise it is not needed.
Released for:Schneider Electric Ireland
Explore more
Product:
LV434063
Range:
ComPacT NSXm, new generation
ComPact NSX
Articles that might be helpful
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.