{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
VW3A1111 used with both ATV320 & ATV630. Print screen stops working

You can use the VW3A1111 to capture an image (jpg) of whatever is shown on screen at the time by using the plain black coloured buttons just below the screen.

vw3a1111, HMI, Drive Keypad

If you press button number 1 on the left and button number 4 on the right at the same time, the screen will flash red for a moment and the screen will be saved on the keypad in a folder called PRTSCN.

You can access these on a computer by connecting via micro USB cable. The keypad will appear as a thumb drive and you can access the folder for PRTSCN directly from there.

You should note that you can only store 20 pictures on the keypad at one time. If you have any storage issues when you have reached this limit, you must delete the PRTSCN folder completely to enable the storage of new files. The next time that you save a screen shot, a new folder will be created automatically.

Schneider Electric Ireland

Explore more
Product:
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: