Search FAQs
Is it possible to use a mix of ZBRT1 and ZBRT2 when using the start/stop function on the ZBRRA receiver?
No, you must use the same type of contact for this function.
When setting the relay for start stop, you first have to teach the two pushbuttons on the same output. You can only complete this step if both pushbuttons have the same types of contact. For best results, use ZBRT1.
If you ever see the below LED signal, it is because you have mixed transmitters on the same output:
![Incompatibility LED display](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000A0Qy1QAF&oid=00DA0000000abSmMAI)
See below video for assistance on setting up the start/stop function.
https://www.se.com/uk/en/faqs/FA361506/
When setting the relay for start stop, you first have to teach the two pushbuttons on the same output. You can only complete this step if both pushbuttons have the same types of contact. For best results, use ZBRT1.
If you ever see the below LED signal, it is because you have mixed transmitters on the same output:
See below video for assistance on setting up the start/stop function.
https://www.se.com/uk/en/faqs/FA361506/
Released for:Schneider Electric Ireland
Attachment(s)
Explore more
Product:
Range:
Explore more
Product:
Range: