Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Acti 9 & IKQ Incomers cable Capacity
125A incomer for both Acti9 & Ikq boards will be max 50mm cable capacity


IKQ switch:

Loadcentre

Acti9 Switch:

Acti9 Switch

160 to 250A Switches & 100A - 250A Mccbs below: (will all come with 400mm extension box)

160A switch which will be 95mm with a lug or a 200A  / 250A which will take 185mm with a narrow palm.

IKQ range: 
IKQ
Acti9 range:
Acti9 250
mccb
100A mccb 95mm with a lug
160A mccb 95mm with a lug
200A mccb 185mm with narrow palm lug
250A mccb 185mm with narrow palm lug 

all snippets from our product brochures please see www.se.com/uk Final Distribution 

 

 

Schneider Electric Ireland

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: